Cookies information
SKF uses cookies on our web site to align the information shown as closely as possible to the visitors' preferences and to tailor our web site user experience in general. By continuing to visit this site you agree to our use of cookies as described in our cookies policy.
The energy industry is under constant pressure in all production environments: conventional or unconventional; onshore or offshore; oil or gas. In the face of rising costs and recent widespread production target misses, exploration and production companies are looking to grow reserves and maximize production—while ensuring safe operations and avoiding environmental impact.
For many decades now, SKF has been at the forefront of upstream and downstrem oil and gas technology. Based on our heritage of over 100 years as global leader in bearing technologies, we’ve made strategic investments over the last 30 years to also become a leading supplier of bearings, sealing systems, lubrication systems, condition monitoring technology and services. In addition, SKF can provide also expert consultancy and asset management services, maintenance tools and trainings.
Both onshore and offshore, above the ocean’s surface and below, most exploration and production facilities are focused on improving the reliability and availability of rotating equipment.
To improve the performance of upstream equipments, SKF has developed solutions and products for Top Drives, Drilling tools, Well stimulation, Well completion, Artificial lift, Mooring system.
| Download SKF Upstream Solutions |
The oil & gas downstream industry has been facing an increasing number of challenges in recent years.
Through our global engineering, reliability and service organization, SKF can provide products and solution for Industrial pumps, Funs and Compressors. SKF protofoliu contains specialized bearing, lubrication system, Condition Monitoring.
| Download SKF Downstream Solutions |
Condition Monitoring: Multilog IMx-8 and IMx-16Plus
SKF Multilog devices provide a complete system for early fault detection. Improve the reliability, availability and performance of your rotating equipment with automatic advice for correcting existing or impending conditions.
| Download Brochure IMx 16 |
Hybrid bearings have rings made of bearing steel and rolling elements made of bearing grade silicon nitride (Si3N4). Because silicon nitride is such an excellent electrical insulator, hybrid bearings can be used to effectively insulate the housing from the shaft in both AC and DC motors as well as in generators.
In addition to being an excellent insulator, hybrid bearings have higher speed capabilities and provide longer bearing service life than standard bearings under the same operating conditions. Hybrid bearings also perform extremely well under vibrating or oscillating conditions.
SKF Speedi-Sleeve and SKF shaft seals
Repair your worn-out shaft in 30 minutes
The new generation SKF Speedi-Sleeve uses a proprietary stainless steel material and manufacturing process, resulting in an optimized seal counterface surface that minimizes wear on both sleeve and sealing lip.
The proprietary material provides increased strength and excellent ductility properties of the sleeve. Imperceptible lubricant pockets enable the lubricant to reside on the sleeve and thereby prevent dry running of the sealing lip that otherwise can create excessive wear.